Request for KV10 sensorless FOC application circuit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Request for KV10 sensorless FOC application circuit

1,259 Views
Alan_AVN
Contributor I

Now I am designing sensorless FOC motor control based on KV10. I survied NXP web site and found AN4935 which based on KV10 Tower board and TWRMCLV3PH. But, it does not provide KV10 FOC real application circuit.
Can anyone provides me KV10 FOC application circuit for reference?  Thanks a lot!

Best regards,

Alan

Labels (1)
0 Kudos
Reply
1 Reply

1,122 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Please combine TWR-KV10Z32 board schematics with TWR-MC-LV3PH board schematics to get PMSM sensorless FOC control circuit.  The demo PMSM motor is Low voltage(24V) type.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply