Request for KV10 sensorless FOC application circuit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Request for KV10 sensorless FOC application circuit

1,312件の閲覧回数
Alan_AVN
Contributor I

Now I am designing sensorless FOC motor control based on KV10. I survied NXP web site and found AN4935 which based on KV10 Tower board and TWRMCLV3PH. But, it does not provide KV10 FOC real application circuit.
Can anyone provides me KV10 FOC application circuit for reference?  Thanks a lot!

Best regards,

Alan

ラベル(1)
0 件の賞賛
返信
1 返信

1,175件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Please combine TWR-KV10Z32 board schematics with TWR-MC-LV3PH board schematics to get PMSM sensorless FOC control circuit.  The demo PMSM motor is Low voltage(24V) type.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信