Regarding USB multilink Universal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding USB multilink Universal

2,193 Views
sheillysharma
Contributor I

Hello,

I am using USB MULTILINK UNIVERSAL tool  and facing problem in programming our kintex k61 micro-controller with part number MK61FX512VMJ12.

When we are trying to program,it's asking for firmware update and i have updated firmware 6.10 and code warrior which i am using is 10.5.
whether i need to update code warrior too.The snap shot of error is attached..
Thanks
Sheilly 
0 Kudos
Reply
1 Reply

2,133 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Please visit the P&E USB Multilink Universal Download link here to download [USB Multilink Universal (and FX) Resource CD], which Contains firmware update utility.

Please check if using that firm ware update utility could fix the issue.

If not, please update the CodeWarrior software to the latest Rev. 10.7

BTW: There is a note about CodeWarrior software doesn't support new Kinetis devices, more detailed info here.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply