Regarding Tx in CAN (KEA128)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Regarding Tx in CAN (KEA128)

1,619 次查看
jashanm
Contributor III

hi all,

       i have initialized the CAN module to work at 500 Kbps, now i have transferred  my buffer data to Tx registers (MSCAN_TEDSRx). i am not able to transmit the data via CAN bus. AM i missing something ??

Regards,

Jashan M

标签 (1)
0 项奖励
回复
1 回复

1,436 次查看
david_diaz
NXP Employee
NXP Employee

Hello Jashan,

Based on the Reference Manual, the procedure to initially start up the MSCAN module out of reset is as follows:

  1. Assert CANE
  2. Write to the configuration registers in initialization mode
  3. Clear INITRQ to leave initialization mode

Besides, I would like to recommend the MSCAN driver for Kinetis EA devices.

In case you are interested please refer to the following link:

KEA |Kinetis KEA Automotive MCUs|Freescale

Finally, the following document could be useful because of the basic concepts.

Bosch Controller Area Network (CAN)

Please let me know if this material is useful for you, in case it is not I will be glad to help.

Have an excellent day.

David