Regarding Tx in CAN (KEA128)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding Tx in CAN (KEA128)

1,607 Views
jashanm
Contributor III

hi all,

       i have initialized the CAN module to work at 500 Kbps, now i have transferred  my buffer data to Tx registers (MSCAN_TEDSRx). i am not able to transmit the data via CAN bus. AM i missing something ??

Regards,

Jashan M

Labels (1)
0 Kudos
Reply
1 Reply

1,424 Views
david_diaz
NXP Employee
NXP Employee

Hello Jashan,

Based on the Reference Manual, the procedure to initially start up the MSCAN module out of reset is as follows:

  1. Assert CANE
  2. Write to the configuration registers in initialization mode
  3. Clear INITRQ to leave initialization mode

Besides, I would like to recommend the MSCAN driver for Kinetis EA devices.

In case you are interested please refer to the following link:

KEA |Kinetis KEA Automotive MCUs|Freescale

Finally, the following document could be useful because of the basic concepts.

Bosch Controller Area Network (CAN)

Please let me know if this material is useful for you, in case it is not I will be glad to help.

Have an excellent day.

David