Recover FRDM K64F

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Recover FRDM K64F

9,438件の閲覧回数
wmmihaa
Contributor I

I've got an FRDM K64F and it's been working fine for weeks. However, I think I've messed something up as I can't mount the board to the USB any more. When I hook it up, nothing happened. I've tried booting it up in bootloader mode and the USB drive came alive so I downloaded the latest firmware and restarted the device but with the same result after I've restarted it.

There is a red led next to the reset button which I don't think was lit before (see image). Matters got even worse as I accepted the defeat and bought another board...and now I have two K64F with the same issue...

Cheers Mikael

ラベル(1)
タグ(1)
0 件の賞賛
返信
10 返答(返信)

7,160件の閲覧回数
wmmihaa
Contributor I

That's what I thought. I've been testing with different bootloaders from OpenSDA and even the once that come with KDS, but the result is pretty much the same:

****************************************************************************************************************************

Open On-Chip Debugger 0.8.0-dev (2015-01-09-16:22)

Licensed under GNU GPL v2

For bug reports, read

  http://openocd.sourceforge.net/doc/doxygen/bugs.html

Info : only one transport option; autoselect 'cmsis-dap'

Error: unable to open CMSIS-DAP device

Error: unable to init CMSIS-DAP driver

Error: Error selecting 'cmsis-dap' as transport

Runtime Error: C:/Freescale/KDS_v3/openocd/bin/..//scripts/kinetis.cfg:3:

in procedure 'script'

at file "embedded:startup.tcl", line 58

in procedure 'interface' called at file "C:/Freescale/KDS_v3/openocd/bin/..//scripts/kinetis.cfg", line 3

****************************************************************************************************************************

If you'd  have a few minutes to spare on a skype meeting - that would be awesome. My skype id is wmmihaa [at] hotmail [com].

Cheers

Mikael

0 件の賞賛
返信

7,160件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Mikael,

Q1: an 'empty' project will do. The point is to get a project flashed which can run out of reset properly.

Q2: no, the board should be in 'normal' mode so you can debug it

online call: one beer :-)

Erich

0 件の賞賛
返信

7,160件の閲覧回数
wmmihaa
Contributor I

I'm going to cry myself to sleep tonight ...

ok... firmware deployed and KDS installed.

Q1: I assume I need to open some sort of project, but which project would that be?

Q2: Should the board be started in bootloader mode?

Using uVision it tells me "Device not found", but in KDS I don't know where to even set the target...

BTW, how much would it cost me to have an online call... :smileywink:

0 件の賞賛
返信

7,160件の閲覧回数
wmmihaa
Contributor I

I installed the 02_OpenSDA_FRDM-K64F_REVB.bin on the bootloader, stared it up like normal and fired up Keil uVision5 but it can't find the device. I tried the 02_OpenSDA_FRDM-K64F_REVD binary with the same result.

BTW, is uVision a different IDE or is it just a new name for Kinetis Design Studio?

0 件の賞賛
返信

7,160件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Mikael,

Keil uVision is a a product from ARM/Keil (proprietary IDE). Kinetis Design Studio (http://www.nxp.com/kds) is a product from NXP (Eclipse based IDE). They are two different things.

Erich

0 件の賞賛
返信

7,160件の閲覧回数
BlackNight
NXP Employee
NXP Employee

For the second option you need to get the Segger Firmware binary from SEGGER - The Embedded Experts - OpenSDA / OpenSDA V2  and drag&drop it to the Bootloader mode/device. Then you have to use a normal SWD/JTAG debugger (e.g. KDS to re-program/get access to the K64F. As mbed does not include a debugger, you cannot use mbed for this. You need a real tool for this.

Erich

0 件の賞賛
返信

7,160件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Mikael,

the red LED is indicating the reset of the K64F, so your device is constantly resetting.

I had that in a few cases too. See

https://mcuoneclipse.com/2014/04/19/recovering-frdm-k64f-mbed-board/

and

https://mcuoneclipse.com/2014/11/10/recovering-the-frdm-k64f-bootloader-or-cloning-the-program-of-a-...

for possible solutions.

Erich

0 件の賞賛
返信

7,160件の閲覧回数
wmmihaa
Contributor I

Thanks Erich,

I found and read your articles before, but I don't have a Segger J-Link :smileysad:

I don't know if it helps, but I think I know what caused the issue(s). I was playing around with a custom bootloader which downloads a new binary and writes it to the flash and reboots the device. The only problem was that the uri to the new binary was wrong and I accidentally flashed the device with the 404 HTML message I got back (yes I know I should have checked the response code...)

0 件の賞賛
返信

7,160件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Ih Mikael,

if the K20/OpenSDA bootloader is still workign, you do not need a dedicated SWD probe to reflash it.

My experience is that the CMSIS-DAP/mbed firmware has issues to get hold of a 'running wild' K64F: in that case it helps if you either drag&drop that .bin file to recover as explained in one of the article, or if you load the Segger OpenSDA firmware on the board/K20 and then recover the K64F with it.

I hope this helps,

Erich

0 件の賞賛
返信

7,160件の閲覧回数
wmmihaa
Contributor I

Reading the articles (again) it seams to be exactly the same issue, but just to make sure I understand you correctly; You wrote "in that case it helps if you either drag&drop that .bin file to recover as explained in one of the article". -Do you mean booting up the board as normal and drop in a HelloWorld binary in the MBED drive? If this is what you mean, I can't do that as I can't access the device after normal boot using USB.

The second option was "if you load the Segger OpenSDA firmware on the board/K20 and then recover the K64F with it." I grabbed the bin file and drag & dropped it to the USB drive after booting on bootloader mode:

bin.jpg

But after I've done that the device appears dead and no USB drive comes up after normal boot.

0 件の賞賛
返信