Reading MAC address TWR-k60N512

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reading MAC address TWR-k60N512

ソリューションへジャンプ
2,732件の閲覧回数
Aigor
Contributor I

Hi,

is there an how to for read mac address of  TWR-SER module?

Thanks

0 件の賞賛
返信
1 解決策
2,308件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

The serial module doesn't have a MAC address (unless it happens to have one stored in non-volatile memory somewhere on it which I don't know about). The MAC address is assigned to the EMAC (in the processor) and not the PHY (which is on the serial module).

 

The following gives some notes about assigning a MAC address:

 

http://www.utasker.com/forum/index.php?topic=21.0

 

Regards

 

Mark

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,309件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

The serial module doesn't have a MAC address (unless it happens to have one stored in non-volatile memory somewhere on it which I don't know about). The MAC address is assigned to the EMAC (in the processor) and not the PHY (which is on the serial module).

 

The following gives some notes about assigning a MAC address:

 

http://www.utasker.com/forum/index.php?topic=21.0

 

Regards

 

Mark

 

 

 

0 件の賞賛
返信
2,308件の閲覧回数
Aigor
Contributor I

Thanks a lot

0 件の賞賛
返信