Reading MAC address TWR-k60N512

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Reading MAC address TWR-k60N512

跳至解决方案
2,726 次查看
Aigor
Contributor I

Hi,

is there an how to for read mac address of  TWR-SER module?

Thanks

0 项奖励
回复
1 解答
2,302 次查看
mjbcswitzerland
Specialist V

Hi

 

The serial module doesn't have a MAC address (unless it happens to have one stored in non-volatile memory somewhere on it which I don't know about). The MAC address is assigned to the EMAC (in the processor) and not the PHY (which is on the serial module).

 

The following gives some notes about assigning a MAC address:

 

http://www.utasker.com/forum/index.php?topic=21.0

 

Regards

 

Mark

 

 

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,303 次查看
mjbcswitzerland
Specialist V

Hi

 

The serial module doesn't have a MAC address (unless it happens to have one stored in non-volatile memory somewhere on it which I don't know about). The MAC address is assigned to the EMAC (in the processor) and not the PHY (which is on the serial module).

 

The following gives some notes about assigning a MAC address:

 

http://www.utasker.com/forum/index.php?topic=21.0

 

Regards

 

Mark

 

 

 

0 项奖励
回复
2,302 次查看
Aigor
Contributor I

Thanks a lot

0 项奖励
回复