Hello Iva,so far I have used the micro of NXP, an example is LPC1768 and through librery lpcwarethat put in provisions functions to configure the uart, the gpiio etc without having to know in detail the register of mcu. was wondering if Freescale has realized functions in c to configure peripherals MCU.Thanks for reply.Antonello
-
Messaggio originale----
Da: ivadorazinova <admin@community.freescale.com>
Data: 21/01/2016 13.20
A: "Antonello Stella"<microlab.l@libero.it>
Ogg: Re: - is there a library for mke04z8vtgr' peripherals?
a
body {
font-family: Helvetica, Arial, sans-serif;
-webkit-text-size-adjust: 100%;
}
h1, h2, h3, h4, h5, h6, p, hr {
-webkit-margin-before: 0;
-webkit-margin-after: 0;
-webkit-margin-start: 0;
-webkit-margin-end: 0;
}
.button td {
background-image: -moz-linear-gradient(top, #75B7E3 0%, #5498D6 50%, #408BD0 51%, #387AC8 100%) !important;
background-image: -webkit-gradient(linear, left top, left bottom, color-stop(0%,#75B7E3), color-stop(50%,#5498D6), color-stop(51%,#408BD0), color-stop(100%,#387AC8)) !important;
-webkit-box-shadow: inset 0 1px 0 #74b9de, 0 1px 3px rgba(0,0,0,.3) !important;
-moz-box-shadow: inset 0 1px 0 #74b9de, 0 1px 3px rgba(0,0,0,.3) !important;
}
-->
NXP Community
is there a library for mke04z8vtgr' peripherals?
reply from Iva Dorazinova in Kinetis Microcontrollers - View the full discussion
Hi Antonello,
please, can you more specify to us your question? What library do you need?
You probably mean MKE04Z8VTG4, right?
Here are Application Notes with related software, please take a look at it
KE04 |Kinetis KE04 48 MHz Robustness MCUs|NXP
Hope this helps.
Best Regards,
Iva
Reply to this message by replying to this email, or go to the message on NXP Community
Start a new discussion in Kinetis Microcontrollers by email or at NXP Community
Following is there a library for mke04z8vtgr' peripherals? in these streams:
Inbox
This email was sent by NXP Community because you are a registered user.
You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences