Re: is there a library for mke04z8vtgr' peripherals?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Re: is there a library for mke04z8vtgr' peripherals?

1,010 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Antonello,

please, can you more specify to us your question? What library do you need?

You probably mean MKE04Z8VTG4, right?

Here are Application Notes with related software,  please take a look at it

KE04 |Kinetis KE04 48 MHz Robustness MCUs|NXP

Hope this helps.

Best Regards,

Iva

0 项奖励
回复
1 回复

814 次查看
anto
Contributor II

Hello Iva,so far I have used the micro of NXP, an example is LPC1768 and through librery lpcwarethat put in provisions functions to configure the uart, the gpiio etc without having to know in detail the register of mcu. was wondering if Freescale has realized functions in c to configure peripherals MCU.Thanks for reply.Antonello

-


Messaggio originale----

Da: ivadorazinova <admin@community.freescale.com>

Data: 21/01/2016 13.20

A: "Antonello Stella"<microlab.l@libero.it>

Ogg: Re: - is there a library for mke04z8vtgr' peripherals?

a

body {

font-family: Helvetica, Arial, sans-serif;

-webkit-text-size-adjust: 100%;

}

h1, h2, h3, h4, h5, h6, p, hr {

-webkit-margin-before: 0;

-webkit-margin-after: 0;

-webkit-margin-start: 0;

-webkit-margin-end: 0;

}

.button td {

background-image: -moz-linear-gradient(top, #75B7E3 0%, #5498D6 50%, #408BD0 51%, #387AC8 100%) !important;

background-image: -webkit-gradient(linear, left top, left bottom, color-stop(0%,#75B7E3), color-stop(50%,#5498D6), color-stop(51%,#408BD0), color-stop(100%,#387AC8)) !important;

-webkit-box-shadow: inset 0 1px 0 #74b9de, 0 1px 3px rgba(0,0,0,.3) !important;

-moz-box-shadow: inset 0 1px 0 #74b9de, 0 1px 3px rgba(0,0,0,.3) !important;

}

-->

NXP Community

is there a library for mke04z8vtgr' peripherals?

reply from Iva Dorazinova in Kinetis Microcontrollers - View the full discussion

Hi Antonello,

please, can you more specify to us your question? What library do you need?

You probably mean MKE04Z8VTG4, right?

Here are Application Notes with related software, please take a look at it

KE04 |Kinetis KE04 48 MHz Robustness MCUs|NXP

Hope this helps.

Best Regards,

Iva

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in Kinetis Microcontrollers by email or at NXP Community

Following is there a library for mke04z8vtgr' peripherals? in these streams:

Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

0 项奖励
回复