Re: Flexbus initialization and test for external SRAM..?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: Flexbus initialization and test for external SRAM..?

2,319 Views
logancheng
Contributor I

Hi, there is also a similar problem on my device. We have added 512 KB external SRAM to our K60n512 board. The initialization function is the same as described above (as the code from Todd) or in AN4393, except the following

// Set FlexBus Base address for CS0.

FB->CS[0].CSAR = 0x70000000;

// Set CS control register for CS0. Addr s&h, 4 WS, AutoAck, 8bit port.

FB->CS[0].CSCR = FB_CSCR_ASET(1) | FB_CSCR_RDAH(1) | FB_CSCR_WS(4) |

          FB_CSCR_AA_MASK | FB_CSCR_PS(1);

// Set FlexBus Base address mask for CS0 and set valid (enable).

FB->CS[0].CSMR = FB_CSMR_BAM(0x07) | FB_CSMR_V_MASK;

When checking FB_CS0 in the oscilloscope while doing some read/write at base address, no signals can be observed from FB_CS0.

It would be appreciated if anyone could provide some possible hints or information about this problem.

0 Kudos
Reply
3 Replies

1,999 Views
Kan_Li
NXP TechSupport
NXP TechSupport

As I know, the flexbus of K60 mapped at the following addresses:

11.png

None of them starts from 0x70000000, so would you please try to change FB->CS[0].CSAR to 0x60000000 or 0x90000000 and try again?

Please kindly let me know if the problem is still there.

0 Kudos
Reply

1,999 Views
logancheng
Contributor I

The problem is solved, CS0 signal can be observed now. After much effort in trying and also checking with hardware designer, we found out it was the following two points that caused the problem:

1. hardware: the address line connection was incorrect on board

2. software:  the base address used during read/write was not correctly written, it should be

#define MRAM_START_ADDRESS (*(vuint8*)(0x70000000))

FB_CSAR0 = (uint32)&MRAM_START_ADDRESS;

and when accessing

.....

*(vuint8*)(&MRAM_START_ADDRESS + n) = wdata8;

rdata8=0x00; //clear data variable;

rdata8=(*(vuint8*)(&MRAM_START_ADDRESS + n));

......

Anyway, many thanks for your reply!

0 Kudos
Reply

1,999 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

I check the Flexbu setting code without any problem.

AN4393 the Flexbus initialization code with below Flexbus clock frequency drivid setting:

SIM_CLKDIV1 |= SIM_CLKDIV1_OUTDIV3(0x0); //FlexBus Clock not divided

Please make sure the Flexbus clock frequency not exceed 50MHz.

Wish it helps.

0 Kudos
Reply