RED LED

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RED LED

2,317 次查看
shivasubramania
Contributor I


Hello,

On plugging the USB port of my FRDM-K22F with my laptop, a RED LED(D2) is continuously ON.  And may be because of none of the example codes been debugged. Can you please guide me to solve this issue. It will be helpful if the solution can be mailed also (@ [email protected] ).

Thanking you in advance. !!!

0 项奖励
回复
3 回复数

1,936 次查看
DavidS
NXP Employee
NXP Employee

Hi Shiva,

Please goto the Freedom board Product Page:

FRDM-K22F|Freedom Development Platform|Kinetis MCU|NXP

Click on the Getting Started tab to see if this helps you.

Regards,

David

0 项奖励
回复

1,936 次查看
shivasubramania
Contributor I

Hi David,

Thanks for your reply. I have gone through the tutorial video but regarding this issue ( Red Led ) nothing special is mentioned.

-S.Shiva

0 项奖励
回复

1,936 次查看
DavidS
NXP Employee
NXP Employee

Hi S. Shiva,

The red LED indicates that the device is in continuous reset state. 

Have you been able to load an application and debug it?

If yes, then red LED should not be on.

If no, then you might need to re-install debugger firmware.

Please review following:

Summary of FRDM-K22F debug interface | NXP Community

With updated debugger firmware (this updates on the K20) you should be able to download application example to the K22.

If red LED still on, then you might have to visually check the board for defect or damage.

Regards,

David

0 项奖励
回复