usb_cdc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

usb_cdc

1,568 Views
sreeramadhanala
Contributor I

Hi,

I am beginner of Codewarrior.

I want to try USB_CDC with MK20 in ProcessorExpert.

But,in FSL_USB_CDC Component,how to add MK20 in cpu popupmenu?(i used usb_stack_4.1.1.)

Thank u

Labels (2)
0 Kudos
Reply
1 Reply

1,403 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Sreerama,

Which K20 MCU are you using? Maybe the following post created by our colleague Erich Styger is helpful for you, it explains the usage of the FRDM-K20D50M as USB CDC with Processor Expert:

https://mcuoneclipse.com/2013/04/27/usb-cdc-with-the-frdm-k20d50m/

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply