Question Regarding Motor control using FRDM-KL25Z

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Question Regarding Motor control using FRDM-KL25Z

跳至解决方案
8,777 次查看
bargavipichai
Contributor I

I need to write a simple program to control a motor using FRDM-KL25Z evaluation board. I am new to this and I have few questions regarding that..

1. Can I connect a motor directly on my board without using motor driver. If so what kind of motor is compatible with the above mentioned board.

2. If I have to connect a motor through motor driver or motor sheild  what kind of motor sheild is compatible with the above mentioned board.

3. I have the evaluation board where can I get motor sheild and motors. Is there any tutorial available for simple motor control programs..

I have also created a service requests for this issue  service req. no. 1-1094510216 , 1-1094337910 I think tech support closed it but I didnt get any answer..

Can someone please answer these questions that would be really helpful.. Thanks a lot!

标记 (2)
0 项奖励
回复
1 解答
5,011 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

for 1): the general answer is no, you cannot connect a motor directly to the board. Because the motor will need too much current.

for 2): Many are compatible. You just need to verify that they work for 3.3V operation. Some motor shields need 5V logic levels, and without a level shifter, they will not work.

for 3): simply search the internet and look at your prefered provider. There are many, many.

But if you want to see what I'm using, here are a few links:

The Freedom Zumo Robot | MCU on Eclipse

Tutorial: Arduino Motor/Stepper/Servo Shield – Part 1: Servos | MCU on Eclipse

Tutorial: Arduino Motor/Stepper/Servo Shield – Part 2: Timed Servo Moves | MCU on Eclipse

Tutorial: Arduino Motor/Stepper/Servo Shield – Part 3: 74HCT595 Shift Register | MCU on Eclipse

Freedom Track Robot with IEEE802.15.4/SMAC | MCU on Eclipse

Maze solving FRDM-KL25Z Robot goes backward for Dead-Ends | MCU on Eclipse

Pololu Line Following Robot with Freedom Board | MCU on Eclipse

I hope this helps.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
5,012 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

for 1): the general answer is no, you cannot connect a motor directly to the board. Because the motor will need too much current.

for 2): Many are compatible. You just need to verify that they work for 3.3V operation. Some motor shields need 5V logic levels, and without a level shifter, they will not work.

for 3): simply search the internet and look at your prefered provider. There are many, many.

But if you want to see what I'm using, here are a few links:

The Freedom Zumo Robot | MCU on Eclipse

Tutorial: Arduino Motor/Stepper/Servo Shield – Part 1: Servos | MCU on Eclipse

Tutorial: Arduino Motor/Stepper/Servo Shield – Part 2: Timed Servo Moves | MCU on Eclipse

Tutorial: Arduino Motor/Stepper/Servo Shield – Part 3: 74HCT595 Shift Register | MCU on Eclipse

Freedom Track Robot with IEEE802.15.4/SMAC | MCU on Eclipse

Maze solving FRDM-KL25Z Robot goes backward for Dead-Ends | MCU on Eclipse

Pololu Line Following Robot with Freedom Board | MCU on Eclipse

I hope this helps.

0 项奖励
回复
5,011 次查看
bargavipichai
Contributor I

Hi Erich-

As I already mentioned in my above email, I need to write a simple program to control a motor using FRDM-KL25Z evaluation board.

I got this seeed studio expand arduino motor sheild and a micro servo motor(voltage 4.8-6V) from radio shack

http://www.trossenrobotics.com/p/grove-motor-shield.aspx?feed=Froogle&gclid=CNK09rzutbgCFWUV7AodVk8A... ( I think this is the only model that is available in the store )

In the motor sheild it is mentioned as

"The motor sheild is a perfect platform for robotics and mechanical applications. It enables the arduino to drivetwo brushed DC motors or one 4-wire two-phase stepper motor. Based on the L298N H-bridge motor driver a 6-15 volt external supply powers the motor. It also includes 5 volt voltage regulator for powering the main arduino board. It includes an onboard 5-volt voltage regulator for powering the main Arduino board.Additional plug and play grove sensors can be connected to the 13 on board Grove connectors.

Features:

Standard Arduino Compatible.

PWM speed control mode.

4-direction indicator lights.

Compatible with Grove plug and play sensors.

Extra large heat sink helps handle big loads.

Supports upto 14 servos.

! This product is not intended to as a standalone product requires Arduino or Seeed components to work".

It means I should not connect the servo motor directly to this motor sheild right?. Have you used this board ? Can I connect the servo motor to this board and control using FRDM-KL25Z?

I looked for the exact same Arduino Motor Sheild you have mentioned in your tutorial part-1 but it is not available in radio shack. Can I find it in any retail stores because in Adafruit it will take around 10 business days to become available.

I don't have any electricals background I am really sorry to bother you with the simple question. I just don't want to blow my board. If possible, can you please help me with this issue?

Thanks a lot!

Regards

Bargavi.

0 项奖励
回复
5,011 次查看
BlackNight
NXP Employee
NXP Employee

Hi Bargavi,

are you talking about DC motors or (hobby) servo motors?

These are two completely different concepts.

For DC motors you need a H-Bridge such as an LH298N (there are many, many similar ones available).

A small hobby servo you could attach directly to the FRDM board, as long it is not dawing too much current. In any case you can use a separate 5V supply or battery for a servo motor.

If you want to rely on Radio Shack for such electronics supply, I think that typically will not work. Get things from one of the many online stores, and many give you same-day-shipping.

As you are new to electronics, have a look at the forum and ressources sites e.g. at pololu.com: they cover many aspects and question you are asking in their tutorials. Or have a look at sparkfun.com too: both ship very fast.

I hope this helps.

Erich

0 项奖励
回复
5,011 次查看
bargavipichai
Contributor I


Hi Erich-

I am planning to buy the below female headers to connect 1 servo motor to FRDM-KL25Z evaluation board. Can you please review and let me know if this is the correct header? Should I have to connect external power supply to connect 1 servo motor [voltage: 4.8-6V]? if yes can you please tell me how to connect it to FRDM-KL25Z board?

http://www.mouser.com/ProductDetail/3M-Electronic-Solutions-Division/929870-01-01-RA/?qs=sGAEpiMZZMs...

Thanks a lot for your time.

Regards

Bargavi

0 项奖励
回复
5,011 次查看
bargavipichai
Contributor I

Hi Erich-

Thanks for the reply and usefull links!

Regards

Bargavi

0 项奖励
回复