Project with FRDM 16KEZ - I2C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Project with FRDM 16KEZ - I2C

1,444 Views
Andrei13
Contributor III

I included the I2C from peripherals but this if def doesn t get trought and the functions in the #if define 

doesn t work when i use the in main.

Andrei13_0-1678351882708.png

 

0 Kudos
Reply
1 Reply

1,417 Views
CarlosGarabito
NXP TechSupport
NXP TechSupport

Hi @Andrei13 that function is not used in the main, this is the head of the code

0 Kudos
Reply