Programming issues with KDS3.0.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programming issues with KDS3.0.0

1,484 Views
tommyb90
Contributor III

Hi to everyone,

I am having some troubles while programming a MK64F on a custom board using JTAG protocol with the P&E micro Multilink Universal.

I am developing using KDS 3.0.0 and the Processor Expert.

I already programmed this chip before and never had any issue, but this time it happens that while trying to flash my program into the chip, the starting address becomes 0xfffffe (usually it was 0x2823 or something similar) and the program is not stored anymore.

It seems like the compilation fails to configure the memory settings, but since last time I edited just one line of code in the main.c file.

Did this happen to anyone else and knows how to solve this?

Thanks in advance,

        Tommaso

0 Kudos
Reply
1 Reply

1,404 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Tommaso,

Could you please first download a simple project to have a try ,check whether there

is some problem about the hardware.

And what about the error after you download the project ?

BR

Alice

0 Kudos
Reply