Programming flash while running code from flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming flash while running code from flash

1,924件の閲覧回数
east_sun
Contributor I

Hi, I use S32DS environment debugging TRK - KEA128 board Flash function, normal in debug mode can erase and write, but can't erase and write in normal mode, need to be copied into ram to run the program?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,509件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi JD Sun,

Please refer the FRDM_KEA128_FLASH_FTMRE example in FRDM-KEA-QSP.(...\FRDM-KEA-QSP\Quick Start Package v8\Code Project Examples and Sample Drivers (Evaluation Grade Only)\FRDM-KEAZ128\Driver Test SW for KEAZ128\Driver Test SW for KEAZ128\FRDM_KEA128_FLASH_FTMRE)

FLASH_LaunchCMD.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,509件の閲覧回数
east_sun
Contributor I

Thank you. What's the way to put Flash code into RAM?

0 件の賞賛
返信