Programming flash while running code from flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programming flash while running code from flash

1,935 Views
east_sun
Contributor I

Hi, I use S32DS environment debugging TRK - KEA128 board Flash function, normal in debug mode can erase and write, but can't erase and write in normal mode, need to be copied into ram to run the program?

Labels (1)
0 Kudos
Reply
2 Replies

1,520 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi JD Sun,

Please refer the FRDM_KEA128_FLASH_FTMRE example in FRDM-KEA-QSP.(...\FRDM-KEA-QSP\Quick Start Package v8\Code Project Examples and Sample Drivers (Evaluation Grade Only)\FRDM-KEAZ128\Driver Test SW for KEAZ128\Driver Test SW for KEAZ128\FRDM_KEA128_FLASH_FTMRE)

FLASH_LaunchCMD.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,520 Views
east_sun
Contributor I

Thank you. What's the way to put Flash code into RAM?

0 Kudos
Reply