Programming K64F board by drag and drop bin./ hex. file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Programming K64F board by drag and drop bin./ hex. file

跳至解决方案
1,303 次查看
grochal7
Contributor III

Hello!

I have one question.

If I programmed my K64F board by using bin. or .hex file and "drag and drop" method will all flash also be erased?

Regards!

1 解答
1,114 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Tomasz Sobiech

It will depend on the OpenSDA debugger interface. Most of the application perform a mass erase before flashing your program.

Hope this helps.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,115 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Tomasz Sobiech

It will depend on the OpenSDA debugger interface. Most of the application perform a mass erase before flashing your program.

Hope this helps.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------