Programming K64F board by drag and drop bin./ hex. file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming K64F board by drag and drop bin./ hex. file

ソリューションへジャンプ
1,900件の閲覧回数
grochal7
Contributor III

Hello!

I have one question.

If I programmed my K64F board by using bin. or .hex file and "drag and drop" method will all flash also be erased?

Regards!

ラベル(2)
1 解決策
1,711件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Tomasz Sobiech

It will depend on the OpenSDA debugger interface. Most of the application perform a mass erase before flashing your program.

Hope this helps.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,712件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Tomasz Sobiech

It will depend on the OpenSDA debugger interface. Most of the application perform a mass erase before flashing your program.

Hope this helps.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------