Processor Expert -> Undefined Reference in Peripheral Init

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert -> Undefined Reference in Peripheral Init

ソリューションへジャンプ
2,952件の閲覧回数
KevinRosenbaum
Contributor I

I'm starting a new Kinetis project with the MKL15Z128VFM4.  I'm using Processor Expert (PE) on another Kinetis project for some lower level peripheral initialization components, but I'm having trouble with this project.  PE compiles fine, but when I include a PDD routine (in my case one of the GPIO or ADC routines) I get an "undefined reference" error to that routine.  If I use the higher level components, it compiles and works fine.  Is there anything obvious I need to setup first?

For example, when I add the following to my main(), I get the error "undefined reference to 'ADC_PDD_StartCalibration'.

ADC_PDD_StartCalibration(ADC0_DEVICE);

I have CW 10.4 and just made sure everything else is up-to-date.

Thanks!

ラベル(1)
0 件の賞賛
返信
1 解決策
2,609件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi KevinRosenbaum,

       After reading your problem, I create a CW project based on PE. After test, I think if you want to use PDD, two points you should take care.Now I still take ADC_PDD as an example.

      1, You should include the PDD.h which you used in your main.c

              If you use the ADC_PDD_StartCalibration(ADC0_DEVICE); Add the following:

                 #include "ADC_PDD.h"

           Because ADC_PDD_StartCalibration() is defined in ADC_PDD.h as follows:

    #define ADC_PDD_StartCalibration(PeripheralBase) ( \

    ADC_SC3_REG(PeripheralBase) |= \

     ADC_SC3_CAL_MASK \

  )

     2, Make sure your ADC0_DEVICE is the correct peripheral base address.

         eg, I use ADC_PDD_StartCalibration(ADC0_BASE_PTR);

       you can find ADC0_BASE_PTR in the IO_Map.h

After these 2 points, I compile the project with no error!

I hope my answer helps you!

Best regards!

Jing

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,610件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi KevinRosenbaum,

       After reading your problem, I create a CW project based on PE. After test, I think if you want to use PDD, two points you should take care.Now I still take ADC_PDD as an example.

      1, You should include the PDD.h which you used in your main.c

              If you use the ADC_PDD_StartCalibration(ADC0_DEVICE); Add the following:

                 #include "ADC_PDD.h"

           Because ADC_PDD_StartCalibration() is defined in ADC_PDD.h as follows:

    #define ADC_PDD_StartCalibration(PeripheralBase) ( \

    ADC_SC3_REG(PeripheralBase) |= \

     ADC_SC3_CAL_MASK \

  )

     2, Make sure your ADC0_DEVICE is the correct peripheral base address.

         eg, I use ADC_PDD_StartCalibration(ADC0_BASE_PTR);

       you can find ADC0_BASE_PTR in the IO_Map.h

After these 2 points, I compile the project with no error!

I hope my answer helps you!

Best regards!

Jing

0 件の賞賛
返信
2,609件の閲覧回数
KevinRosenbaum
Contributor I

That was it.  Thank you!

0 件の賞賛
返信
2,609件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport
you are welcome!
0 件の賞賛
返信