Processor Expert and Keil uVision

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert and Keil uVision

ソリューションへジャンプ
3,670件の閲覧回数
hl
Contributor II

Hi community,

I try to generate a K70 project for Keil uVision by Processor Expert ("New",->"Processor Expert project"...), but the "Expert" do not provide to select that type

as target compiler.

The option I get are:

1. CodeWarrior ARM

2. GNU C

3. IAR ARM

No Keil uVision...

The PE version: 10.0.0

Any idea, what's wrong?

Regards,

HL

ラベル(1)
0 件の賞賛
返信
1 解決策
3,152件の閲覧回数
apanecatl
Senior Contributor II

Yes, the problem is that the last version of PE does not generate initialization/configuration code for Keil uVision

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,153件の閲覧回数
apanecatl
Senior Contributor II

Yes, the problem is that the last version of PE does not generate initialization/configuration code for Keil uVision

0 件の賞賛
返信
3,152件の閲覧回数
hl
Contributor II

It's a pity...

Is it planned, to correct this?

Regards,

HL

0 件の賞賛
返信
3,152件の閲覧回数
PetrC
Contributor II

Hello

There is a problem in the new project wizard. Please create the K70 project for any other compiler. When project is created, you can select the Keil compiler in the cpu component setting on the Build Options tab.

PetrPExDrv_K70.jpg

0 件の賞賛
返信
3,152件の閲覧回数
hl
Contributor II

Hi Petr,

thanks for the hint.

HL

0 件の賞賛
返信
3,152件の閲覧回数
apanecatl
Senior Contributor II

So far there are no plans to add the support for Keil uVision

0 件の賞賛
返信