Processor Expert and Keil uVision

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Processor Expert and Keil uVision

跳至解决方案
3,722 次查看
hl
Contributor II

Hi community,

I try to generate a K70 project for Keil uVision by Processor Expert ("New",->"Processor Expert project"...), but the "Expert" do not provide to select that type

as target compiler.

The option I get are:

1. CodeWarrior ARM

2. GNU C

3. IAR ARM

No Keil uVision...

The PE version: 10.0.0

Any idea, what's wrong?

Regards,

HL

标签 (1)
0 项奖励
回复
1 解答
3,204 次查看
apanecatl
Senior Contributor II

Yes, the problem is that the last version of PE does not generate initialization/configuration code for Keil uVision

在原帖中查看解决方案

0 项奖励
回复
5 回复数
3,205 次查看
apanecatl
Senior Contributor II

Yes, the problem is that the last version of PE does not generate initialization/configuration code for Keil uVision

0 项奖励
回复
3,204 次查看
hl
Contributor II

It's a pity...

Is it planned, to correct this?

Regards,

HL

0 项奖励
回复
3,204 次查看
PetrC
Contributor II

Hello

There is a problem in the new project wizard. Please create the K70 project for any other compiler. When project is created, you can select the Keil compiler in the cpu component setting on the Build Options tab.

PetrPExDrv_K70.jpg

0 项奖励
回复
3,204 次查看
hl
Contributor II

Hi Petr,

thanks for the hint.

HL

0 项奖励
回复
3,204 次查看
apanecatl
Senior Contributor II

So far there are no plans to add the support for Keil uVision

0 项奖励
回复