Processor Expert and Keil uVision

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor Expert and Keil uVision

Jump to solution
3,623 Views
hl
Contributor II

Hi community,

I try to generate a K70 project for Keil uVision by Processor Expert ("New",->"Processor Expert project"...), but the "Expert" do not provide to select that type

as target compiler.

The option I get are:

1. CodeWarrior ARM

2. GNU C

3. IAR ARM

No Keil uVision...

The PE version: 10.0.0

Any idea, what's wrong?

Regards,

HL

Labels (1)
0 Kudos
Reply
1 Solution
3,105 Views
apanecatl
Senior Contributor II

Yes, the problem is that the last version of PE does not generate initialization/configuration code for Keil uVision

View solution in original post

0 Kudos
Reply
5 Replies
3,106 Views
apanecatl
Senior Contributor II

Yes, the problem is that the last version of PE does not generate initialization/configuration code for Keil uVision

0 Kudos
Reply
3,105 Views
hl
Contributor II

It's a pity...

Is it planned, to correct this?

Regards,

HL

0 Kudos
Reply
3,105 Views
PetrC
Contributor II

Hello

There is a problem in the new project wizard. Please create the K70 project for any other compiler. When project is created, you can select the Keil compiler in the cpu component setting on the Build Options tab.

PetrPExDrv_K70.jpg

0 Kudos
Reply
3,105 Views
hl
Contributor II

Hi Petr,

thanks for the hint.

HL

0 Kudos
Reply
3,105 Views
apanecatl
Senior Contributor II

So far there are no plans to add the support for Keil uVision

0 Kudos
Reply