Problems with Launchinng New_configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems with Launchinng New_configuration

1,402件の閲覧回数
charli18p
Contributor I

hey, I have a problem when I try to debug my program with codewarrior(version 10.6):

WhatsApp Image 2019-09-25 at 5.55.46 PM.jpeg

How can I sove that?

Thanks. 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,317件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Carlos Castillo,

   What's the debugger you are using?

   You need to select the correct debugger in your debugger configuration, then you can download it.

    I think you can create a simple CW project for KL25, and choose the related debugger when you create the project, then generate the code, build the project and download it again.

   Please try it.

    If you still have questions about it, please kindly let  me know.

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信