Problems with FRDM-KL25Z quickstart

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems with FRDM-KL25Z quickstart

1,767 Views
marciomello
Contributor I

Hello!

My first time using a Freescale kit. In QuickStart guide, to load an Open SDA Application, it says:

" Copy & paste or drag & drop the MSD Flash Programmer Application (MSD-FRDM-KL25Z_vXYZ_Pemicro.SDA)to the BOOTLOADER drive."

But when I try to copy, it just goes till 70% of copying and crashes.

Can someone help me?

Labels (1)
2 Replies

1,573 Views
marciomello
Contributor I

Hey Erich,

Im using a Win7, and it is really giving me problems to paste. Your method didn't work just with the first document I tried, the rest went ok.

Thanks a lot!    

1,573 Views
BlackNight
NXP Employee
NXP Employee

Hi,

Which host operating system are you using?

Can you try to copy the file using the DOS command shell (instead of copy/paste with the windows explorer)?

It might be that you are using an explorer extension which causes problems.

(see OpenSDA on the Freedom KL25Z Board)

I hope this helps.

0 Kudos
Reply