Problems while using TIMERS in mkl25z128vlk4??????

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems while using TIMERS in mkl25z128vlk4??????

1,974件の閲覧回数
akshayhv
Contributor II

i m trying to write a timers code using interrupts but i m not sure of how to generate a delay of my requirements can only one please help me out on thi   

regards

Akshay H V

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,722件の閲覧回数
Monica
Senior Contributor III

Hello Akshay,

please don't forget to tell us how's it going! Did it work?

Best regards,

Monica.

0 件の賞賛
返信

1,722件の閲覧回数
antonioconcio
NXP Employee
NXP Employee

Hi Akshay,

You can use Processor Expert to generate code, it is very simple. In your case, in order to generate an interrupt every X time, you can only add the "TimerInt_LDD" components and set the Interrupt period (see image below); in addition you can set the source and set if you wish the Timer Auto or Manual Initialization.

Capture.PNG

Regards,

Antonio