Problems running K60FN1 tower with FNET code.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problems running K60FN1 tower with FNET code.

1,533 次查看
flacca
Contributor II

I'm looking for some suggestions on resolving very sluggish performance on the ethernet link. I have downloaded the example K60 shell code from the fnet site and it seems to be running fine on the tower. I have the K60 configured to run with a 120mhz core clock and the ethernet chip on the SER board is setup for RMII using the 50mhz clock. When I ping the tower from my PC I very rarely get 4 good replies without a time-out. Not sure how to resolve this....any debug suggetstions out there?

0 项奖励
回复
1 回复

1,399 次查看
mjbcswitzerland
Specialist V

Hi Frank

Unreliability usually stems from the 50MHz clock source - check the jumpers carefully again and verify with the setups recommended in http://www.utasker.com/docs/KINETIS/uTaskerV1.4_Kinetis_demo.pdf (chapter 7).

If you have the TWR-K60F120M check with the binary at http://www.utasker.com/kinetis/TWR-K60F120M.html

Regards

Mark

Kinetis: µTasker Kinetis support

K60: µTasker Kinetis TWR-K60N512 support / µTasker Kinetis TWR-K60D100M support / µTasker Kinetis TWR-K60F120M support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 项奖励
回复