K60 MMA7760 Accelerometer with I2C Protocol

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K60 MMA7760 Accelerometer with I2C Protocol

1,953件の閲覧回数
broccolee
Contributor III

Does anybody know how to output the K60 tower board's accelerometer measurements via I2C Protocol and ProcessorExpert? I tried the example in codewarrior, debugged it, but it only returns descriptions, not measurements:

K60_MMA7660.jpg

Any help, suggestions, guides on how to program this would be very much appreciated This is work related and time-sensitive.

Thanks,

Dao.

0 件の賞賛
返信
2 返答(返信)

1,439件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Dao,

What a pity!

There are no demos that integrate K60 with MMA7760 for you, however I found a PE demo about KL25 usage another three-axis acccelerometer MMA8451Q.

The MMA84Q1 also support the I2C proposal and the demo is very worth to referring to.

I've attached the demo with the reply and please check it.
Have a great day,

Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,439件の閲覧回数
broccolee
Contributor III

Thanks for your help.

0 件の賞賛
返信