Problems detecting ports for OpenSDA in Kinetis Design Studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems detecting ports for OpenSDA in Kinetis Design Studio

3,978 Views
alexanderabrica
Contributor II

Hi, I'm testing my new FRDM-KL25Z; but when I try to debug my project, the debugging is incomplete because there isn't a port that can make the operation finish. Even when I select the OpenSDA (usb) or any other interface for the FRDM-KL25Z, nothing aperce in the options for the port.

pastedImage_2.png

4 Replies

3,422 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Alexander,

Please first update the firmware in booltoader mode use the attachment file .

The process is like this :

(1) Unplug the USB (OpenSDA port ) cable if attached.

(2) Press and hold the Reset button (SW1). Plug in a USB cable . Release the Reset button.

(3)  Copy & paste  "DEBUG-APP_Pemicro_v102.SDA" ( the attachment)  to the BOOTLOADER drive.

(4)  Unplug the USB cable and plug it in again.

Then open the KDS again , click the refresh button to have a try :

pastedImage_1.pngpastedImage_2.png

Also pay attention to the usb connect to the OpenSDA port .

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,422 Views
ce_2015
Contributor I

Thanks so much! I've been at this for hours and you just solved it!

0 Kudos
Reply

3,422 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi,

Welcome !

BR

Alice

0 Kudos
Reply

3,422 Views
alexanderabrica
Contributor II

Thank you very much Alice :smileygrin:

0 Kudos
Reply