Problems debugging FRDM-K66F with Seeger J-Link Plus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems debugging FRDM-K66F with Seeger J-Link Plus

2,763 Views
ChristofAbt
Contributor II

Good morning,

I want to use the Seeger J-Link plus to debug the MK66FN2M8VMD18 on my FRDM-K66F evaluation board via the SWD debug interface. This interface consists of two signals SWDIO and SWCLK. Unfortunately your wording used in the schematic SPF-28682_REV B.pdf does not correspond to the standard. There are the signals SWD_SDA_TGTMCU, TRACE_SWO, JTAG_TDO/TRACE_SWO/EZP_DO/FTM0_CH7. Which of these signals correspond to the standard SWD signals. I attached the error report additionally. An experienced user could probably detect the fault. 

0 Kudos
Reply
3 Replies

2,747 Views
Habib_MS
NXP Employee
NXP Employee

Hello @ChristofAbt,
PTA0 and PTA3 corresponds to SWD standard signals:

Habib_MS_4-1743199757570.pngHabib_MS_4-1743199757570.png

And are used in the SDW connector:

Habib_MS_5-1743199890331.pngHabib_MS_5-1743199890331.png

These are designed to support JTAG and SWD, also, as mentioned in the chapter 3.2 called "Series and debug adapter (OpenSDAv2.1)" in the Freedom FRDM-K66F Development Platform User’s Guide. These signals are also brought out to a standard 10-pin (0.05”) Cortex Debug connector (J9). I highly recommend see this chapter in order to obtain more information.
BR
Habib

0 Kudos
Reply

2,676 Views
ChristofAbt
Contributor II

Thanks for the quick reply but please use the naming standards in your schematics.

Best regards Christof

0 Kudos
Reply

2,665 Views
Habib_MS
NXP Employee
NXP Employee

Hello again @ChristofAbt

Thank you for the feedback, I will share the comments to the hardware design team. So, they can deliberate about the addition of this on a future.

BR
Habib.

0 Kudos
Reply