Problem with reset pin KV4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with reset pin KV4

1,319件の閲覧回数
petrzbranek
Contributor I

Hi,

ラベル(1)
1 返信

1,149件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Petr,

Were you able to flash the MCU once? Maybe the problem is related to the SWD connection and not with the configuration of the pin, the recommended SWD connection is the following:

pastedImage_0.png

It is also recommended to place a 100 nF capacitor in the RESET_b pin close to the MCU for transient protection and an external 4.7 kΩ to 10 kΩ pullup resistor.

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------