Problem with macros in mk22f51212.h from SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with macros in mk22f51212.h from SDK

1,024 Views
Keith4DSmith
Contributor V

Attached is my copy of mk22f51212.h from the Kinetis SDK for K22F Freedom board, v2.3.1.

Structures defining various base register types, such as SIM_Type or  RTC_Type, etc. are properly defined.

The macros that are used to extract bit fields from these structures seem to be wrong.

The intent appears to be to move the bit field in the low order bits of uint32_t variable.

However, the shift operator << should be >>.

Am I missing something? Is there some big endian/little endian issue I don't understand?

Example:

#define SIM_SOPT1_RAMSIZE_MASK (0xF000U)
#define SIM_SOPT1_RAMSIZE_SHIFT (12U)
#define SIM_SOPT1_RAMSIZE(x) (((uint32_t)(((uint32_t)(x)) << SIM_SOPT1_RAMSIZE_SHIFT)) & SIM_SOPT1_RAMSIZE_MASK)

===================================================================

#include "MK22F51212.h"

SIM_Type *pSIM = (SIM_Type*)SIM_BASE;

uint32_t ram_size = SIM_SOPT1_RAMSIZE(pSIM->SOPT1);

============================================================================

ram_size returns zero as the bit field is shifted the wrong direction.

Tags (1)
0 Kudos
Reply
2 Replies

891 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi  Keith:

The macro is used to write a value into a register. Not for reading.

For example, if the ram size is 512.

Then with macro  SIM_SOPT1_RAMSIZE, you can set the  relative bit field to 512.

Regards

Daniel

891 Views
Keith4DSmith
Contributor V

Thank you. I knew I was missing something.

0 Kudos
Reply