Problem with interrupts in a KL17Z256 processor.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problem with interrupts in a KL17Z256 processor.

跳至解决方案
2,568 次查看
peterabdelmassi
Contributor I

Dear all.

I am trying to configure different interrupts on a KL 17Z256 processor ( KSDK1.0.0 and Kinetis 2.0 IDE.) but run into problems when several interrupts arrive within a short time frame. My main loop then simply get stuck.

Hence I have some questions.

1) Are nestled interrupts enabled as default, that is, will my ISR routine get interrupted for other interrupts of higher prio?

2) Do I need to run PORT_HAL_ClearPinIntFlag after entering the ISR, or is this handled by itself. I have seen many different ideas about this on the internet, and in ARMs documention they state that the flag is cleared after entering the ISR.

Kind Regards

Peter Abdelmassih Waller

标签 (1)
0 项奖励
回复
1 解答
2,407 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Peter,

1) Are nestled interrupts enabled as default, that is, will my ISR routine get interrupted for other interrupts of higher prio?

    Yes, the lower interrupt will be preempted by the higher interrupt.

2) Do I need to run PORT_HAL_ClearPinIntFlag after entering the ISR, or is this handled by itself. I have seen many different ideas about this on the internet, and in ARMs documention they state that the flag is cleared after entering the ISR.

    You need to use the PORT_HAL_ClearPinIntFlag function to clear the status of the GPIO interrupt.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,406 次查看
peterabdelmassi
Contributor I

Another question...if only higher prio interrupts lower prio, then nested interrupts are not "turned on" in my case since I didnt change any priorities and they are problaby all equal (zero??). 

Is correct then that only system interrupts (not possible to change prio on those) that will interrupt my onging ISRs?

Kind Regards

Peter

0 项奖励
回复
2,406 次查看
peterabdelmassi
Contributor I

Hi Jeremy,

thank you for your support, it will surely help in the troubleshooting.

Is it correct that an interrupt will not be preempted by another one with the same priority?

Kind Regards

Peter

0 项奖励
回复
2,406 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Peter,

Thanks for your reply.

1) Is it correct that an interrupt will not be preempted by another one with the same priority?

    No.

And I'd highly recommend you to learn the more information about the NVIC from the ARM website whose link is below.

ARM Information Center
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,408 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Peter,

1) Are nestled interrupts enabled as default, that is, will my ISR routine get interrupted for other interrupts of higher prio?

    Yes, the lower interrupt will be preempted by the higher interrupt.

2) Do I need to run PORT_HAL_ClearPinIntFlag after entering the ISR, or is this handled by itself. I have seen many different ideas about this on the internet, and in ARMs documention they state that the flag is cleared after entering the ISR.

    You need to use the PORT_HAL_ClearPinIntFlag function to clear the status of the GPIO interrupt.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复