Problem with TWR-K64F120M and TWR-SER ethernet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with TWR-K64F120M and TWR-SER ethernet

ソリューションへジャンプ
1,545件の閲覧回数
kalden_srcinc
Contributor IV

I am having trouble getting the KSDK 1.1.0 lwIp ping demo running on the TWR-K64F120M.  I have set all the jumpers on the two boards according to this document: http://cache.freescale.com/files/microcontrollers/doc/user_guide/TWRK64F120MUG.pdf

I believe the intention is to configure TWR-SER for RMII and enable the 50MHz clock to be routed up to the K64.  With the jumpers in this configuration, I cannot get my program to main.  here is the gdb output:

(gdb) b main

Breakpoint 1 at 0x8df4: file /home/kalden/Freescale/KSDK_1.1.0/demos/lwip_ping_demo/ping_rtos/src/ping.c, line 286.

(gdb) c

Continuing.

^C

Program received signal SIGTRAP, Trace/breakpoint trap.

0x00008f6c in SystemInit () at /home/kalden/Freescale/KSDK_1.1.0/platform/startup/MK64F12/system_MK64F12.c:237

237    while((MCG->S & MCG_S_IREFST_MASK) != 0x00U) {

Now, If I remove J32 and connect J33 on the TWR-K64, the software seems to run as expected.  I just don't see any packets coming out of the board.  It is my understanding that populating J33 uses the K64 onboard clock.  J32 disables this and should use the 50MHz clock from TWR-SER.  Could I be missing a jumper setting somewhere?  I'm not sure where to go from here.

Thanks

1 解決策
1,353件の閲覧回数
kalden_srcinc
Contributor IV

Well this is embarrassing.  I had the TWR-SER in backwards :smileyhappy:   All is well now.

元の投稿で解決策を見る

1 返信
1,354件の閲覧回数
kalden_srcinc
Contributor IV

Well this is embarrassing.  I had the TWR-SER in backwards :smileyhappy:   All is well now.