Problem using KWIKSTIK-K40

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem using KWIKSTIK-K40

Jump to solution
1,881 Views
hardeepsingh
Contributor II

I'm using Kinetis KWIKSTIK-K40 demo board where I'm facing problems while programming the device. When I connect it say USB device not recognized. Tried to give the path of the .inf file for driver but it did not install the driver and hence, I'm not able to program the Flash on the device. Please suggest what shall I do to resolve it.

Labels (2)
0 Kudos
Reply
1 Solution
1,671 Views
CarlosCasillas
NXP Employee
NXP Employee

Hello,

Have you ensured which Kwikstik version do you have? Have you verified if this case corresponds to the described on “KWIKSTIK_07: Failure to Power from J-Link USB” section of the KwikStik-K40 Hardware Errata Rev. 5 document, available at the following link:

www.freescale.com/files/32bit/doc/errata/KWIKSTIKK40HWER.pdf


Hope this will be useful for you.

Best regards!

/Carlos

View solution in original post

0 Kudos
Reply
1 Reply
1,672 Views
CarlosCasillas
NXP Employee
NXP Employee

Hello,

Have you ensured which Kwikstik version do you have? Have you verified if this case corresponds to the described on “KWIKSTIK_07: Failure to Power from J-Link USB” section of the KwikStik-K40 Hardware Errata Rev. 5 document, available at the following link:

www.freescale.com/files/32bit/doc/errata/KWIKSTIKK40HWER.pdf


Hope this will be useful for you.

Best regards!

/Carlos

0 Kudos
Reply