Problem to program KL05Z - reset_b oscillation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem to program KL05Z - reset_b oscillation

3,110件の閲覧回数
R_L_
Contributor I

Hi All,

     I'm having problems to program a KL05z . The board has only a 3.3v regulator  and a conection to SDA bus. I'm using  Keil + U-Multilink + KL05Z.

    

     I follow the guidelines of other posts (hold the reset_b to gnd during the powerup) but the MCU doesn't go to program mode.

     I read that this situation is normal before the first programming , but I don't know what i'm doing wrong.

I send a picture of the reset_b pin :

TEK0000.JPG.jpg

does exist a procedure to resolve this issue ?

Thanks in advance for your help.

Best Regards

Rodrigo

タグ(4)
0 件の賞賛
返信
3 返答(返信)

2,525件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Rodrigo,

Please check the RESET_b pin related circuit, if there with a 10K ohm pull-up resistor with RESET_b pin? And if you refer FRDM_KL05Z board to use  1UF capacitor? If so, could you try to modify the capacitor value to 0.1uF or just remove that capacitor.

Wish it helps.

B.R.

Ma Hui

0 件の賞賛
返信

2,525件の閲覧回数
lachlanaudas
Contributor I

Got  the same problem on a MKL04Z32VLF4,   debug works..    step's etc

but the  reset pin is oscillating!   pulling it hi with 100 Ohms resistor to 3.3v a pear’s to stop it oscillating ,   but,  cut it (while powered).. and oscillation is back !..  :smileysad:

Lachlan

0 件の賞賛
返信

2,525件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Lachlan,


"If flash is not programmed, the reset vector is 0xFFFF,FFFF , it is a illegal address, may cause reset. In reset sequence, reset pin will drive out"

So the waveform you observed is an expected behavior.

You can program KL04 chip with available image, then you could find the reset pin oscillating behavior gone.

Wish it helps.

Best regards,

Ma Hui

0 件の賞賛
返信