Problem sending data if length is les than usb in endpoint

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem sending data if length is les than usb in endpoint

1,417件の閲覧回数
PedroBecerra
Contributor III

I'm using cdc comunication with USB stack 4.1.1 and I have problems if the string I wnat to send is smaller or equal to the In Endpoint size.

If my string is longer everything is ok.

If my string is equal never is sent.

If my string is shorter it's sent 3 or 4 times and after I never can send anything more.

At the moment I've made a workarround and if the string length is les than endpoint size I complete it with 0x00. And this way it works perfect. But this is not a solution. On the other side of the cominication I should throw away those 0x00 and maybe some of them could be part of my message.

0 件の賞賛
返信
1 返信

1,199件の閲覧回数
mjbcswitzerland
Specialist V

Hi

If you prefer simple, fast and reliable CDC (rather than fixing the examples) just get it from here: http://www.utasker.com/kinetis.html

There are many binaries showing CDC with up to 6 USB-UART bridges and composites (probably one will run on boards you use).
5 year track record in many industrial Kinetis based products (and more in Coldfires).

All Kinetis devices are simulated, with accurate USB emulation to avoid any quess work.

Regards

Mark

Guides:
http://www.utasker.com/docs/uTasker/uTaskerV1.3_USB_Demo.PDF
http://www.utasker.com/docs/uTasker/USB_User_Guide.PDF
Also use for RNDIS - http://www.utasker.com/docs/uTasker/uTaskerRNDIS.pdf

0 件の賞賛
返信