Problem While reading AC current parameter using Shunt Type with SADC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem While reading AC current parameter using Shunt Type with SADC

2,282 Views
avinashbhavsar
Contributor I

I am working on Energy Meter Micro controller IC MKM34Z256VLQ7

Now I am stuck while reading current parameter from SADC 24 bit and getting SADC count with more variation and not seen any repetition while testing with 0 to 500mv

I have tested rang of 0 to 500mV voltage by applying DC volt and its working well with this with no variation .

But variation occur with the AC parameter only .

Please help if any some have any idea about this .

Hardware reference DRM122.

0 Kudos
Reply
1 Reply

2,170 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Avinash Bhavsar,

     This question is the repeat post, I already answer you in your another post which have the same question, please refer to it:

Problem While reading AC current using Shunt Type with SADC  

Any updated information, please reply me in that post.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply