Powering unused DDR module?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Powering unused DDR module?

ソリューションへジャンプ
2,911件の閲覧回数
alistairhill
Contributor I

I am using a MK61FN1M0VMJ15 however I am not using the DDR module at all, do I need to apply power to the VDD_DDR pins


Thanks


Alistair

ラベル(1)
タグ(1)
1 解決策
2,555件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Alistair

If you do not use DDR function, You don’t need to power DDR_VDD and DDR_VREF. You can leave them floating.

Hope my reply can help you.

Best Regards

Paul

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,555件の閲覧回数
Monica
Senior Contributor III

Hello Alistair,

how's the project going? Did you make any progress? Keep us posted! :smileywink:

Regards,

Monica

0 件の賞賛
返信
2,555件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Alistair

If you do not use DDR function, You don’t need to power DDR_VDD and DDR_VREF. You can leave them floating.

Hope my reply can help you.

Best Regards

Paul

0 件の賞賛
返信
2,555件の閲覧回数
alistairhill
Contributor I

This is exactly the answer I was hoping for

Thanks

Alistair