Powering unused DDR module?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Powering unused DDR module?

Jump to solution
2,911 Views
alistairhill
Contributor I

I am using a MK61FN1M0VMJ15 however I am not using the DDR module at all, do I need to apply power to the VDD_DDR pins


Thanks


Alistair

Labels (1)
Tags (1)
1 Solution
2,555 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Alistair

If you do not use DDR function, You don’t need to power DDR_VDD and DDR_VREF. You can leave them floating.

Hope my reply can help you.

Best Regards

Paul

View solution in original post

0 Kudos
Reply
3 Replies
2,555 Views
Monica
Senior Contributor III

Hello Alistair,

how's the project going? Did you make any progress? Keep us posted! :smileywink:

Regards,

Monica

0 Kudos
Reply
2,555 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Alistair

If you do not use DDR function, You don’t need to power DDR_VDD and DDR_VREF. You can leave them floating.

Hope my reply can help you.

Best Regards

Paul

0 Kudos
Reply
2,555 Views
alistairhill
Contributor I

This is exactly the answer I was hoping for

Thanks

Alistair