Power the USB Controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power the USB Controller

2,578 Views
loicguillain
Contributor II

Capture.PNG

Hi everybody,

I'm using a K64 microcontroller with a battery charger, battery and an external regulator. By consequence i don't use the usb regulator VREGIN pin and the VOUT33 pin to supply my circuit (it works very well). However, now i want to use the USB controller to communicate with a computer by USB. I was wondering how can I do to supply voltage to the USB Controller. Can I connect VOUT33 and VDD together to do this? Am i forced to use the USB regulator?

I would appreciate an help :smileyhappy:

Thanks to you.

Labels (2)
0 Kudos
Reply
3 Replies

2,317 Views
loicguillain
Contributor II

FRDM-K64

I'm testing the USB SDA port to communicate with Tera Term and turn a led off thank to my keyboard, it works.

Now i would like to same thing with the other USB port (Shield_K64USB). Problem: Not recognized by my computer as a com port, is it normal? If yes how can i do?

Thanks a lot!

0 Kudos
Reply

2,317 Views
loicguillain
Contributor II

I know connecting VOUT33 and VDD (where i have my 3.3v output from my external regulator) = having 3.3v going on the usb regulator output...

0 Kudos
Reply

2,317 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Loic Guillain:

The USB transceiver gets its power from the internal USB regulator, so you need to connect the VREGIN input to either VBUS line or VDD power and also the output capacitor on VOUT33.

Supplying the USB transceiver from the VOUT33 pin is not an option.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------