Possible bug in USB 5.0 stack, in usb_dev.c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Possible bug in USB 5.0 stack, in usb_dev.c

1,524 Views
johnstrohm
Contributor III

In file usb_dev.c, routine usb_device_recv_data() contains the following:

    OS_Mutex_lock(usb_dev_ptr->mutex);

    /* Initialize the new transfer descriptor */

    xd_ptr->ep_num = ep_num;

    xd_ptr->bdirection = USB_RECV;

    xd_ptr->wtotallength = size;

    xd_ptr->wstartaddress = buff_ptr;

    xd_ptr->wsofar = 0;

    xd_ptr->bstatus = USB_STATUS_TRANSFER_ACCEPTED;

    if (((usb_dev_interface_functions_struct_t*)\

       usb_dev_ptr->usb_dev_interface)->dev_recv != NULL)

    {

        error = ((usb_dev_interface_functions_struct_t*)\

                 usb_dev_ptr->usb_dev_interface)->dev_recv(usb_dev_ptr->controller_handle, xd_ptr); 

    }

    else

    {

        #if _DEBUG

        printf("usb_device_recv_data: DEV_RECV is NULL\n");                     

        #endif   

        return USBERR_ERROR;

    }

    OS_Mutex_unlock(usb_dev_ptr->mutex);

Observe that the dev_recv() function pointer is NULL, the mutex will be left locked.  This will probably have bad consequences down the road.

Observing that there is no point in setting up the transfer descriptor and locking the mutex if the transfer routine is missing, may I suggest the following revision?

    if (((usb_dev_interface_functions_struct_t*)\

       usb_dev_ptr->usb_dev_interface)->dev_recv != NULL)

    {

        OS_Mutex_lock(usb_dev_ptr->mutex);

        /* Initialize the new transfer descriptor */

        xd_ptr->ep_num = ep_num;

        xd_ptr->bdirection = USB_RECV;

        xd_ptr->wtotallength = size;

        xd_ptr->wstartaddress = buff_ptr;

        xd_ptr->wsofar = 0;

        xd_ptr->bstatus = USB_STATUS_TRANSFER_ACCEPTED;

        error = ((usb_dev_interface_functions_struct_t*)\

                 usb_dev_ptr->usb_dev_interface)->dev_recv(usb_dev_ptr->controller_handle, xd_ptr); 

        OS_Mutex_unlock(usb_dev_ptr->mutex);

    }

    else

    {

        #if _DEBUG

        printf("usb_device_recv_data: DEV_RECV is NULL\n");                     

        #endif   

        return USBERR_ERROR;

    }

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

1,306 Views
makeshi
NXP Employee
NXP Employee

Thanks for you raising the issue, it is a real  issue in USB stack, USB software team will fix
it in subsequent release.

0 Kudos
Reply