Possible bug in USB 5.0 stack, in usb_dev.c

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Possible bug in USB 5.0 stack, in usb_dev.c

1,599件の閲覧回数
johnstrohm
Contributor III

In file usb_dev.c, routine usb_device_recv_data() contains the following:

    OS_Mutex_lock(usb_dev_ptr->mutex);

    /* Initialize the new transfer descriptor */

    xd_ptr->ep_num = ep_num;

    xd_ptr->bdirection = USB_RECV;

    xd_ptr->wtotallength = size;

    xd_ptr->wstartaddress = buff_ptr;

    xd_ptr->wsofar = 0;

    xd_ptr->bstatus = USB_STATUS_TRANSFER_ACCEPTED;

    if (((usb_dev_interface_functions_struct_t*)\

       usb_dev_ptr->usb_dev_interface)->dev_recv != NULL)

    {

        error = ((usb_dev_interface_functions_struct_t*)\

                 usb_dev_ptr->usb_dev_interface)->dev_recv(usb_dev_ptr->controller_handle, xd_ptr); 

    }

    else

    {

        #if _DEBUG

        printf("usb_device_recv_data: DEV_RECV is NULL\n");                     

        #endif   

        return USBERR_ERROR;

    }

    OS_Mutex_unlock(usb_dev_ptr->mutex);

Observe that the dev_recv() function pointer is NULL, the mutex will be left locked.  This will probably have bad consequences down the road.

Observing that there is no point in setting up the transfer descriptor and locking the mutex if the transfer routine is missing, may I suggest the following revision?

    if (((usb_dev_interface_functions_struct_t*)\

       usb_dev_ptr->usb_dev_interface)->dev_recv != NULL)

    {

        OS_Mutex_lock(usb_dev_ptr->mutex);

        /* Initialize the new transfer descriptor */

        xd_ptr->ep_num = ep_num;

        xd_ptr->bdirection = USB_RECV;

        xd_ptr->wtotallength = size;

        xd_ptr->wstartaddress = buff_ptr;

        xd_ptr->wsofar = 0;

        xd_ptr->bstatus = USB_STATUS_TRANSFER_ACCEPTED;

        error = ((usb_dev_interface_functions_struct_t*)\

                 usb_dev_ptr->usb_dev_interface)->dev_recv(usb_dev_ptr->controller_handle, xd_ptr); 

        OS_Mutex_unlock(usb_dev_ptr->mutex);

    }

    else

    {

        #if _DEBUG

        printf("usb_device_recv_data: DEV_RECV is NULL\n");                     

        #endif   

        return USBERR_ERROR;

    }

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,381件の閲覧回数
makeshi
NXP Employee
NXP Employee

Thanks for you raising the issue, it is a real  issue in USB stack, USB software team will fix
it in subsequent release.

0 件の賞賛
返信