Position-Independent Code example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Position-Independent Code example

ソリューションへジャンプ
4,223件の閲覧回数
publius
Contributor II

Hi,

Does anybody know where I can download the code example discussed in AN5163 "Load Position-Independent Code (PIC) on a Kinetis Platform Using the IAR EWARM Compiler"?

Thanks

ラベル(1)
1 解決策
3,684件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please download the AN5163 related software from here.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,684件の閲覧回数
vlastimilsetka
Contributor I

Hi, is it something like described in AN5163 "Load Position-Independent Code ..." also possible with GCC? There are -fPIC anf -fPIE gcc options, but it seems these are intended for something a bit different.

0 件の賞賛
返信
3,684件の閲覧回数
bobpaddock
Senior Contributor III

The short answer is 'No'.  

0 件の賞賛
返信
3,685件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please download the AN5163 related software from here.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,684件の閲覧回数
publius
Contributor II

Thanks

0 件の賞賛
返信