Position-Independent Code example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Position-Independent Code example

Jump to solution
4,236 Views
publius
Contributor II

Hi,

Does anybody know where I can download the code example discussed in AN5163 "Load Position-Independent Code (PIC) on a Kinetis Platform Using the IAR EWARM Compiler"?

Thanks

Labels (1)
1 Solution
3,697 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please download the AN5163 related software from here.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
3,697 Views
vlastimilsetka
Contributor I

Hi, is it something like described in AN5163 "Load Position-Independent Code ..." also possible with GCC? There are -fPIC anf -fPIE gcc options, but it seems these are intended for something a bit different.

0 Kudos
Reply
3,697 Views
bobpaddock
Senior Contributor III

The short answer is 'No'.  

0 Kudos
Reply
3,698 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please download the AN5163 related software from here.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,697 Views
publius
Contributor II

Thanks

0 Kudos
Reply