Porting SPI Driver to Keil RL-ARM System: UnInit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Porting SPI Driver to Keil RL-ARM System: UnInit

1,494 Views
tfrauenrath
Contributor III

My task is to port a NXP SPI driver delivered with Keil RL-ARM to my Kinetis K60 system. Finlay I want to talk to SD cards in SPI mode. I do this step by step. My next task is the UnInit routine.

This is the original NXP UnInit:

/* Return SSP interface to default state. */

static BOOL UnInit (void) {

  IODIR0 &= ~(1<<20);

  PINSEL1 &= ~0x000003FC;

  SSPCR1 = 0x0000;

  SSPCR0 = 0x0000;

  SSPCPSR = 0x00;

  return (__TRUE);

}

This my first trial for the Kinetis UnInit:


/*--------------------------- UnInit ----------------------------------------*/

static BOOL UnInit (void) {

/* Return SSP interface to default state. */

PORTD->PCR[11] = PORT_PCR_MUX(1);     /* Alt 1 for GPIO*/

PORTD->PCR[12] = PORT_PCR_MUX(1);     /* Alt 1 for GPIO*/

PORTD->PCR[13] = PORT_PCR_MUX(1);     /* Alt 1 for GPIO*/

PORTD->PCR[14] = PORT_PCR_MUX(1);     /* Alt 1 for GPIO*/

SIM->SCGC3 &= ~SIM_SCGC3_SPI2_MASK;    /* Disable SPI2 gate clocking        */

SIM->SCGC5 &= ~SIM_SCGC5_PORTD_MASK;   /* Disable PORTD gate clocking        */

   

return (__TRUE);

}


Do you think this is applicable for SD card access via SPI?

I will discuss the other routines in other threads because of a better overview. I will post the final driver, because Keil provides only samples for SDHC mode for memory cards for the Kinetis system.

Thank you


Labels (1)
Tags (5)
0 Kudos
Reply
0 Replies