Porting Code from MK20DX256VLH7 to MK20DX256VLL10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Porting Code from MK20DX256VLH7 to MK20DX256VLL10

1,687 Views
SilentBob
Contributor I

Hello,

we thinking about the port our project to the MK20DX256VLL10. (https://www.nxp.com/part/MK20DX256VLL10#/)

 

Apperently this MCU has only one 16-bit timer. 

The MCU that we currently are using (https://www.nxp.com/part/MK20DX256VLH7#/) has 13 16-bit timer. 

Is that correct that the VLL10 has only 1 timer?

0 Kudos
Reply
3 Replies

1,664 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @SilentBob ,

I'm not sure which timer module do you mean MK20DX256VLL10 has three FlexTimer and one LPTMR.

 

Regards,

Jing

0 Kudos
Reply

1,659 Views
SilentBob
Contributor I

Hello, 

I'm using these timers with the MK20DX256VLH7:

#

Timer

 

1

PIT0

 

2

PIT1

 

3

PIT2

 

4

PIT3

 

5

FTM0

 

6

FTM1

 

 

Would that be possible with the VLL10?

0 Kudos
Reply

1,645 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @SilentBob ,

Yes, no problem.

 

Regards,

Jing

0 Kudos
Reply