PinOUT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PinOUT

5,462 Views
1410385858
Contributor I
MKV46F256VLL16  芯片的 外部 时钟输入 引脚 位置 在Pinout中 没有标示 ,请问在那两个 引脚 
0 Kudos
Reply
8 Replies

5,352 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Wang Ming,

    Please check the reference manual: 11.5 KV4x Signal Multiplexing and Pin Assignments

pastedImage_6.png

Wish it helps you!

 

If you still have any question about it, please let me know.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you h

-------------------------------------------------------------------------------

0 Kudos
Reply

5,352 Views
1410385858
Contributor I

thanks a lot !!!

0 Kudos
Reply

5,352 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ming,

   You are welcome!

    If you still have question about it, please kindly let me know.

   If your question is solved, please help me to mark the correct answer, just to close this case, thank you!


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

5,352 Views
1410385858
Contributor I

dear Kerry:

at first , I can not find "Mark Correct" button in the community.

then , i have another question ,: I want to product 6 channel PWM signal to control motor , but I can not make sure the right out pins.

whare I can get sample code or driver soft abut PWM control. thanks a lot.

the MCU is MKV42F256VLL16 .

0 Kudos
Reply

5,352 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Wang ming,

   For the detail PWM pin, you can use the PWM module, which you can find it from chapter Chapter 37
Pulse Width Modulator.  pin is 37.3.1 PWM[n]_A and PWM[n]_B - External PWM Output Pair.

You also can use the FTM module, the channel is FTM_CHn

Wish it helps you.

If you can't find the correct button, you also can mark the helpful or the like button.


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

5,352 Views
Ben
Senior Contributor I

Hello Ming,

If you want to use a motor with H-bridge, you should use complementary mode of the PWM .

See in the chip Referance Manual section 38.3.1:

38.3.1 PWM[n]_A and PWM[n]_B - External PWM Output Pair:
These pins are the output pins of the PWM channels. These pins can be independent
PWM signals or a complementary pair.

Ben

5,352 Views
1410385858
Contributor I

but I can not find the pin function in the pin out list.

0 Kudos
Reply

5,352 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Wang,

   Maybe you can consider the FTM channel, then you can find the pin function still in the reference manual:

11.5 KV4x Signal Multiplexing and Pin Assignments


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply