Pin CS2 in flexbus is not configured in MK66FN2M0.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pin CS2 in flexbus is not configured in MK66FN2M0.

875件の閲覧回数
nataliyadoni
Contributor I

I have worked with MK60FN1M0. My project worked well. Now I'm trying to adapt my project for MK66FN2M0.

I see from Reference manuals that flexbus in MK60 and Mk66 is configured equally.

I use Flexbus cs0,cs2 and cs4. Cs0 and cs4 work correctly but cs2 does not appear. I see FB_ALE, FB_RW  for FB_CS2. But there is no cycles on FB_CS2. I have tried to use PORTC_PCR18(FB_CS2) as GPIO and  in such mode pin worked correctly.

I have tried on two circuit boards but result is the same.

Why cs2 does not appear? Why Pin PTC18 works only as GPIO?

Here the code of initialization:

FB_CSPMCR = FB_CSPMCR_GROUP4(1) ;//0x00010000;// cs0 cs2 cs4

//address/Data

PORTB_PCR20=PORT_PCR_MUX(5); //fb_ad[31]

PORTB_PCR21=PORT_PCR_MUX(5); //fb_ad[30]

PORTB_PCR22=PORT_PCR_MUX(5); //fb_ad[29]

PORTB_PCR23=PORT_PCR_MUX(5); //fb_ad[28]

PORTC_PCR15=PORT_PCR_MUX(5); //fb_ad[24]

PORTC_PCR14=PORT_PCR_MUX(5); //fb_ad[25]

PORTC_PCR13=PORT_PCR_MUX(5); //fb_ad[26]

PORTC_PCR12=PORT_PCR_MUX(5); //fb_ad[27]

PORTB_PCR6=PORT_PCR_MUX(5); //fb_ad[23]

PORTB_PCR7=PORT_PCR_MUX(5); //fb_ad[22]

PORTB_PCR8=PORT_PCR_MUX(5); //fb_ad[21]

PORTB_PCR9=PORT_PCR_MUX(5); //fb_ad[20]

PORTB_PCR10=PORT_PCR_MUX(5); //fb_ad[19]

PORTB_PCR11=PORT_PCR_MUX(5); //fb_ad[18]

PORTB_PCR16=PORT_PCR_MUX(5); //fb_ad[17]

PORTB_PCR17=PORT_PCR_MUX(5); //fb_ad[16]

PORTB_PCR18=PORT_PCR_MUX(5); //fb_ad[15]A15

PORTC_PCR0=PORT_PCR_MUX(5); //fb_ad[14]A14

PORTC_PCR1=PORT_PCR_MUX(5); //fb_ad[13]A13

PORTC_PCR2=PORT_PCR_MUX(5); //fb_ad[12]A12

PORTC_PCR4=PORT_PCR_MUX(5); //fb_ad[11]A11

PORTC_PCR5=PORT_PCR_MUX(5); //fb_ad[10]A10

PORTC_PCR6=PORT_PCR_MUX(5); //fb_ad[9]A9

PORTC_PCR7=PORT_PCR_MUX(5); //fb_ad[8]A8

PORTC_PCR8=PORT_PCR_MUX(5); //fb_ad[7]A7

PORTC_PCR9=PORT_PCR_MUX(5); //fb_ad[6]A6

PORTC_PCR10=PORT_PCR_MUX(5); //fb_ad[5]A5

PORTD_PCR2=PORT_PCR_MUX(5); //fb_ad[4]

PORTD_PCR3=PORT_PCR_MUX(5); //fb_ad[3]A3

PORTD_PCR4=PORT_PCR_MUX(5); //fb_ad[2]A2

PORTD_PCR5=PORT_PCR_MUX(5); //fb_ad[1]A1

PORTD_PCR6=PORT_PCR_MUX(5); //fb_ad[0]

//control signals

PORTC_PCR19=PORT_PCR_MUX(6); //fb_TA_b

PORTC_PCR11=PORT_PCR_MUX(5); //fb_rw_b

PORTD_PCR1=PORT_PCR_MUX(5); //fb_cs0_b

PORTD_PCR0=PORT_PCR_MUX(5); //fb_ale

PORTC_PCR18=PORT_PCR_MUX(5); //fb_cs2

PORTC_PCR17=PORT_PCR_MUX(5); //fb_cs4

PORTB_PCR19=PORT_PCR_MUX(5); //fb_oe

PORTD_PCR8=PORT_PCR_MUX(6); //A16

PORTD_PCR9=PORT_PCR_MUX(6); //A17

PORTD_PCR10=PORT_PCR_MUX(6); //A18

PORTD_PCR11=PORT_PCR_MUX(6); //A19

PORTD_PCR12=PORT_PCR_MUX(6); //A20

SIM_SOPT2 |= SIM_SOPT2_FBSL(3);//разрешение обращения к данным

  /* Enable the clock to the FlexBus module */

        SIM_SCGC7 |= SIM_SCGC7_FLEXBUS_MASK;

Enable the FB_CLKOUT function on PTC3 (alt5 function) */

  PORTC_PCR3 = PORT_PCR_MUX(0x5);

FB_CSAR2 = EXT_START_ADDRESS;

/* Enable CS signal */

FB_CSCR2=0;

FB_CSCR2 |= FB_CSCR_EXTS(1)|FB_CSCR_WRAH(3)|FB_CSCR_RDAH(3)|FB_CSCR_PS(1)|FB_CSCR_WS(24)|FB_CSCR_AA_MASK;

FB_CSMR2 = FB_CSMR_BAM(0x1);

FB_CSMR2 |= FB_CSMR_V_MASK;     

0 件の賞賛
返信
1 返信

781件の閲覧回数
nataliyadoni
Contributor I

I solve my problem.  I undestood that setting SIM_SCGC7_FLEXBUS_MASK  clears the register  FB_CSPMCR.

So after SIM_SCGC7 |= SIM_SCGC7_FLEXBUS_MASK I set the stroke FB_CSPMCR = FB_CSPMCR_GROUP4(1) .

0 件の賞賛
返信